DUG_Exxact Multiwire Push-button Dimmer_WH-00

For your safety

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Safe electrical installation must be carried out only by skilled professionals. Skilled professionals must prove profound knowledge in the following areas:
- Connecting to installation networks.
- Connecting several electrical devices.
- Laying electric cables.
- Safety standards, local wiring rules and regulations.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The output may carry electric current even when the load is switched Off.
Disconnect the device from the supply by switching Off the upstream circuit breaker before working on the device or on the load.
Failure to follow these instructions will result in death or serious injury.
NOTICE
HAZARD OF EQUIPMENT damage
- Only connect dimmable load.
- Ensure that the device is disconnected from its circuit during the insulation resistance test.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?