DUG_Exxact Relay Switch_WH-01

Quick Home Connect

Quick Home Connect is a wireless connectivity solution for Zigbee devices without the need for a Hub or smartphone application. Quick Home Connect is your starting point for wireless home automation. It performs functions like switching, dimming and shutter control using the Connected Wireless Switch (hereinafter referred to as Wireless switch) via a Zigbee network.

The Wireless switch is a battery-powered wireless push-button switch that is used to control Zigbee devices (such as dimmer, shutter, switch, and socket) within the same Zigbee network.

Limitations

  • Quick Home Connect serves only as a room control solution.

  • With a 1-gang Wireless switch, you cannot mix lighting and shutter control. However, with a 2-gang Wireless switch, you can assign one gang for dimming/switching and the other for shutter control, or vice versa.

  • This solution does not support remote control, smartphone app usage, or scheduling features.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.