DUG_Exxact Relay Switch_WH-01

Pairing Wireless Switch with Relay Switch

  1. Short press the upper push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.

  2. Short press the push-button of the Relay Switch 5 times in quick succession.
    The status LED blinks green.

    The light connected to the Relay Switch blinks for a few times. The status LED stops blinking green on the Wireless switch and the Relay Switch. The Relay Switch can now be controlled by the Wireless switch.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.