DUG_LK FUGA Wiser Multiwire Rotary Dimmer_WH-02

About the device

The LK FUGA® Wiser Multiwire LED Rotary Dimmer (hereinafter referred to as dimmer) has a rotary knob that can be used to switch and dim ohmic, inductive or capacitive loads manually or remotely.

Control options

Home control: To control the dimmer through the Wiser Home app, you will need the Wiser Hub.

Direct operation: The dimmer can always be controlled directly on-site. You can also connect any number of mechanical push buttons.

Room control / Quick Home Connect: The dimmer can operate without the Wiser Hub or a smartphone application.

Functions

  • The device can detect the load automatically.

  • The device has internal self-protection, including thermal protection, overload resistance, short-circuit protection, soft start, and soft stop.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.