DUG_LK FUGA Wiser Multiwire Rotary Dimmer_WH-02

Operating a Dimmer

You can switch the dimmer on/off and adjust its brightness using the paired Wireless switch.
  • Short press the left or right of the Wireless switch (< 0,5 s) to turn on/off the connected load (A).

  • Long press the left or right of the Wireless switch (> 0,5 s) to increase or decrease the brightness of the connected load (B).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.