DUG_Odace PB Dimmer_WH-05

About the device

The Connected Universal Push Button Dimmer LED (hereinafter referred to as dimmer) is a push-button device that can be used to switch and dim LED, ohmic, inductive or capacitive loads manually or remotely.

Control options

Home control: To control the dimmer through the Wiser Home app, you will need the Wiser Hub.

Direct operation: The dimmer can always be controlled directly on-site. You can also connect any number of mechanical push buttons.

Functions

  • The device can detect the load automatically.

  • The device has internal self-protection, including thermal protection, overload resistance, short-circuit protection, soft start, and soft stop.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?