DUG_Odace PB Dimmer_WH-05

Using the device

The Device Control Screen allows you to switch ON/OFF the device and control various settings.

On the Control tab, select the dimmer and the control screen shows the options below.


A

Drag the sliding bar up/down to increase/ decrease the brightness.

B

Tap to manually turn the device ON/OFF.

C

Tap to redirect you to the Schedule screen, where you can create a schedule. For more information, refer to the Setting up a schedule topic.

D

Tap to control various settings from the Device Settings screen. For more information, refer to the Configuring the device topic.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?