DUG_Odace Rotary Dimmer_WH-05

Technical Data

Nominal voltage

AC 230 V ~, 50 Hz

Nominal power

Load type Load name Load value

LED

LED

7–100 VA

7–20 VA

Iron core transformer

14–150 VA

Incandescent lamp

14–200 W

Halogen lamp

14–150 W

Electronic step-down converter

14–150 VA

Standby

Max 0.4 W

Neutral conductor

Not required

Connecting Terminals

Screw terminals for max. 2 x 2.5 mm², 0.5 Nm

Extension unit

Single Push-button, unlimited number, max. 50 m

Fuse protection

16 A circuit breaker

Operating frequency

2405 - 2480 MHz

Max. radio-frequency power transmitted

< 10 mW

Communication protocol

Zigbee 3.0 certified

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?