DUG_Ovalis Shutter_WH-07

About the device

You can use the Connected Blind Control Switch (hereinafter referred to as blind control switch) to control a blind or a roller shutter motor that is equipped with end position switches.

Control options

Home control using Wiser Home app: To control the blind control switch through the Wiser app you will need the Wiser Hub. Refer to Pairing the device with the Wiser Hub

Direct operation: The blind control switch can always be controlled directly on-site. You can also connect it with mechanical double push-buttons. Refer to Manual operation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.