DUG_Ovalis Shutter_WH-06

Setting the threshold temperature

Using the Wiser Home app, you can define the inside and outside temperature of a room above which the shutters shall close.

To set the threshold inside and outside temperature:
  1. In the Seasonal Comfort Mode set-up page, tap Temperature.
  2. Set the inside and outside desired temperatures and tap Set.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?