Showing 1,061 - 1,070 of 1,648 results

Page 107 of 165
  • Ställa in timern för rörelsedetektering

    ARGUS rörelsesensor utomhus 360 – Bruksanvisning för Wiser Home-enhet

  • Technical data

    ARGUS Motion Sensor Outdoor 360 – Wiser Home Device user guide

    . LED load Max. number of LED lamps -20 °C to 45 °C 10 A 300 W 15 45 °C to 50 °C 8 A 300 W 15 50 °C to 55 °C 6 A 300 W 15 Relative humidity 0 % to 95 %, non condensing Lux setting 1 lx to 2000 lx, Day mode Night mode Sensitivity setting 1 – 6 (50 % - 100 %) Dimensions Ø 82 mm x 107 mm Ø 82 mm x 131 mm with corner bracket Compliance Communication protocol Zigbee ® 3.0 (certified)
  • Configuring the device

    Unica - Connected Universal Rotary Dimmer LED – Wiser Home Device User Guide

    . B Location: Tap to assign the Dimmer to any room (such as living room, bedroom, kitchen etc). Refer to Setting the device location for more details on how to set the location. C RL-LED Mode: You can improve the dimming quality in the app if you have problems with light flickering. Tap the toggle
  • Configuring the device

    Odace - Connected Universal Rotary Dimmer LED – Wiser Home Device User Guide

    . B Location: Tap to assign the Dimmer to any room (such as living room, bedroom, kitchen etc). Refer to Setting the device location for more details on how to set the location. C RL-LED Mode: You can improve the dimming quality in the app if you have problems with light flickering. Tap the toggle
  • Konfigurera ett schema

    Wiser dimmerpuck LED – Användarhandbok för Wiser Home-enhet

  • Configurar uma programação

    PowerTag Control – Guia do utilizador do dispositivo

  • Einrichten eines Zeitplans

    PowerTag Control – Geräte-Benutzerhandbuch

  • Creating an Account

    Wiser Home – System User Guide (Germany, Austria)

    account to have control over the Wiser system. Refer to the chapter Setting-up the Wiser System for information on how to setup the wiser system. If the homeowner decides to set up the Wiser system independently, they need to begin by creating an account before proceeding with setting up the Wiser
  • Creating an Account

    Wiser Home – System User Guide (Spain and Portugal)

    account to have control over the Wiser system. Refer to the chapter Setting-up the Wiser System for information on how to setup the wiser system. If the homeowner decides to set up the Wiser system independently, they need to begin by creating an account before proceeding with setting up the Wiser
  • Schneider Inverter and Boost Wiser Home Device user guide

    information on Setting Tariff, refer to the respective System UserGuide. Wiser Home AIUse the Wiser Home app, to view device control and schedules. The Wiser Home AI feature automatically schedules high energy consumptiondevices to run during lowest electricity rates, helping in savings on electricity
Page 107 of 165