Showing 1,081 - 1,090 of 1,449 results

Page 109 of 145
  • LED indications

    Wiser Plug – Wiser Home Device User Guide

    , after 60 seconds, the quick blue flashes are followed by 6 slow flashes. Pairing Plug to the Wiser Hub Press ON/OFF button Quick blue flashes followed by 6 slow blue flashes. Pairing mode interruption Press and hold the ON/OFF button for 5 s. 6 slow blue flashes. Reset the Plug and return to factory settings
  • Setting LED brightness

    Wiser Smoke Alarm - 230 V – Wiser Home Device user guide

    Setting LED brightness Setting LED brightness Setting LED brightness You can change the LED brightness to minimum and maximum manually and also using the Wiser Home app. Changing the LED brightness manually When the smoke alarm is in standby mode, short press the Test/Hush button 3 times within 2 s
  • About the device

    LK FUGA® Wiser wireless dimmer – Wiser Home Device User Guide

    options Home control: To control the dimmer through the Wiser Home app you will need the Wiser Hub. Direct operation: The dimmer can always be controlled directly on-site. Functions Automatic load detection. Switch between RC and RL mode. Thermal protection, overload-resistant, short-circuit protection, soft start, soft stop.
  • Setting LED brightness

    Wiser Smoke Alarm - Battery – Wiser Home Device user guide

    Setting LED brightness Setting LED brightness Setting LED brightness You can change the LED brightness to minimum and maximum manually and also using the Wiser Home app. Changing the LED brightness manually When the smoke alarm is in standby mode, short press the Test/Hush button 3 times within 2 s
  • Managing shutter operation without temperature sensor

    Odace - Connected Blind Control Switch – Wiser Home Device user guide

    reference temperature: In the Seasonal Comfort Mode set-up page, tap Other room sensors. Wiser Home app displays the rooms without temperature sensors in list (A). Select a room from the list (A). You can use one of the following temperatures as a reference temperature for the selected room: Temperature
  • LED indication

    Schneider Charge – Wiser Home Device user guide

    access point activated for commissioning Blinking Blue Pairing mode with anti-tripping module (peak controller) activated Blinking Red Anti-tripping module power line communication or TIC communication (France only) lost
  • Setting the room temperature manually

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    “ –” button to decrease the temperature setpoint. In P3, P5, P6, if floor sensor is fitted, device will be in room temperature with floor limits mode. When the room temperature is at or above the current setpoint, the floor temperature is below the lower floor temperature limit (min. guard), the demand is
  • Managing shutter operation without temperature sensor

    Ovalis - Connected Blind Control Switch – Wiser Home Device user guide

    reference temperature: In the Seasonal Comfort Mode set-up page, tap Other room sensors. Wiser Home app displays the rooms without temperature sensors in list (A). Select a room from the list (A). You can use one of the following temperatures as a reference temperature for the selected room: Temperature
  • Managing shutter operation without temperature sensor

    Unica - Connected Blind Control Switch – Wiser Home Device user guide

    reference temperature: In the Seasonal Comfort Mode set-up page, tap Other room sensors. Wiser Home app displays the rooms without temperature sensors in list (A). Select a room from the list (A). You can use one of the following temperatures as a reference temperature for the selected room: Temperature
  • Modo de carregamento

    EVlink Home Smart – Manual do utilizador do dispositivo doméstico Wiser

    Charging Mode, selecione uma das seguintes opções: Manual: Para iniciar o processo de carregamento imediatamente após a ligação à tomada de um veículo elétrico. Reduzir a minha fatura: Para iniciar automaticamente o carregamento durante a próxima ranhura rentável disponível, com base nos detalhes da
Page 109 of 145