DUG_Unica Shutter_WH-08

Managing shutter operation without temperature sensor

Using the Wiser Home app, you can manage the shutter operation of a room where no temperature sensor is installed.

To define the reference temperature:
  1. In the Seasonal Comfort Mode set-up page, tap Other room sensors.
    NOTE: Wiser Home app displays the rooms without temperature sensors in list (A).
  2. Select a room from the list (A).
  3. You can use one of the following temperatures as a reference temperature for the selected room:
    • Temperature detected by temperature sensor of another room.

    • Average temperature detected by all the temperature sensors at home.

    1. To use the temperature of another room as the reference temperature select a room from the list (B).

      NOTE: The temperature of the selected room will be considered as the reference temperature.

    2. To use the average temperature detected by all the temperature sensors as the reference temperature:

      1. Tap Use average home temp (C).


      2. Tap Yes, i’m sure.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?