DUG_Smoke alarm AC_WH-03

Setting LED brightness

You can change the LED brightness to minimum and maximum manually and also using the Wiser Home app.

Changing the LED brightness manually

  1. When the smoke alarm is in standby mode, short press the Test/Hush button 3 times within 2 s.

  2. When the Red LED is On, short press the Test/Hush button to switch between Min. and Max. LED brightness.

  3. Again short press the Test/Hush button 3 times within 2 s to store the adjusted brightness level. Otherwise, you can wait 30 s for the standby LED to turn off, then the brightness level will be saved.

Changing the LED brightness using app

  1. On the Home screen, tap .

  2. Tap Devices > Smoke Alarm > LED Indicator (A).

  3. Short press Setup/Reset (S/R) button on the device to wake it before changing the brightness level.

  4. In the app, select one of the following (B):

    • Maximum

    • Minimum

  5. Tap OK.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?