DUG_LK FUGA Wiser wireless dimmer_WH-00

About the device

The LK FUGA® Wiser wireless dimmer (hereinafter referred to as dimmer) is a push-button device that can be operated locally at the associated operating panel. The dimmer can be used to switch and dim LED, ohmic, inductive or capacitive loads.

The top-left push button turns the light on and increases brightness, while the top-right push button turns the light off and decreases brightness. The bottom push buttons function as a wireless switch. You can configure the actions or moments of the wireless switch using the Wiser Home app.

Control options

Home control: To control the dimmer through the Wiser Home app you will need the Wiser Hub.

Direct operation: The dimmer can always be controlled directly on-site.

Functions

  • Automatic load detection.

  • Switch between RC and RL mode.

  • Thermal protection, overload-resistant, short-circuit protection, soft start, soft stop.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.