Showing 1,101 - 1,110 of 1,622 results

Page 111 of 163
  • Lademodus

    EVlink Home Smart – Wiser Home Gerät Benutzerhandbuch

    Lademodus Lademodus Lademodus Mit der Wiser Home App können Sie den Lademodus verwalten. Tippen Sie auf der Registerkarte Steuerung auf Alle Geräte > EVlink Home Smart. Tippen Sie auf der Bedienfeldseite des Geräts auf Lademodus. Wählen Sie im Menü EV Charging Mode eine der folgenden Optionen
  • LK FUGA® Wiser wireless dimmer

    Mode Setting up the Dimming Mode Dimming Mode allows you to configure how the dimmer operates based on the type of connected lighting load. This feature helps optimize performance and prevent issues such as flickering or overheating. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France
  • Programmes

    Wiser Home – Guide de l’utilisateur du système (France)

    conséquent, si un nouvel événement est ajouté à l’appareil ou si un fonctionnement manuel se produit alors qu’une action programmée est en cours, le système interrompt le programme en cours. Pour une compréhension détaillée du mode d'action/de commande qui a priorité sur les autres, consultez le
  • Configuring the device

    LK FUGA® Wiser wireless dimmer – Wiser Home Device User Guide

    device. B Location: Tap to assign the device to any room (such as living room, bedroom, kitchen etc). For more information, refer to Setting the device location. C Dimming Mode: This setting allows you to improve the dimming quality in the app if you have problems with light flickering. For more
  • Mureva EVlink Wiser Home Device User Guide

    ..................................................................................................15Charging mode...................................................................................16Wiser Home AI ...................................................................................17Anti-Tripping Management
  • Klimatstyrning

    Wiser Home – Systemanvändarhandbok (Sverige, Finland)

    radiatortermostater öppnas/stängs baserat på kommandot). Enskilda enheter kan låsas för manuell drift. Ta bort en klimatenhet från en klimatstyrning genom att ta bort klimatenheten från rummet. Klimatstyrning: A Boost-läge B Måltemperatur C Statusikon Uppvärmningsikon: Kylningsikon: D Uppmätt
  • Wiser Window/Door Sensor Wiser Home Device user guide

    ...................................................................12Selecting the operating mode...............................................................13 Using the device.......................................................................................15Checking the device history
  • Creating an automation

    System M and System D - Connected Push-button Module, 1-gang/2-gang – Wiser Home Device user guide

    change (Select the device): An automation will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more
  • Creating an automation

    Unica - Connected Universal Push-button Dimmer LED – Wiser Home Device User Guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. Refer to the Away Mode topic in the respective System
  • Creating an automation

    Unica - Connected Blind Control Switch – Wiser Home Device user guide

    change (Select the device): An automation will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more
Page 111 of 163