Showing 1,111 - 1,120 of 1,622 results

Page 112 of 163
  • Creating an automation

    Exxact - Connected Blind Control Switch – Wiser Home Device user guide

    change (Select the device): An automation will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more
  • Creating an automation

    LK FUGA Wiser Multiwire LED Rotary Dimmer – Wiser Home Device User Guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. Refer to the Away Mode topic in the respective System
  • Création d’un automatisme

    Odace - Poussoir variateur connecté universel LED 2 fils / 3 fils – Wiser Home Dispositif Guide de l'utilisateur

    . Mode Absence (activez ou désactivez) : Le mode Absence peut également déclencher un automatisme pour allumer les lumières, fermer les volets, etc. Reportez-vous à la rubrique Mode Absence dans le Guide de l’utilisateur du système correspondant. Vous pouvez ajouter jusqu’à 10 conditions. Dans cet
  • Creating an automation

    LK FUGA Wiser Multiwire LED Push-button Dimmer – Wiser Home Device user guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. Refer to the Away Mode topic in the respective System
  • Configuring the device

    Exxact - Connected Motion Sensor with Multiwire Dimmer – Wiser Home Device user guide

    the name of the device. B Location: Tap to assign the device to any room (such as living room, bedroom, kitchen etc). For more information, refer to Setting the device location. C RL-LED Mode: You can improve the dimming quality in the app if you have problems with light flickering. Tap the toggle
  • Configuring the device

    LK FUGA® Wiser wireless PIR dimmer with neutral – Wiser Home Device user guide

    the name of the device. B Location: Tap to assign the device to any room (such as living room, bedroom, kitchen etc). For more information, refer to Setting the device location. C RL-LED Mode: You can improve the dimming quality in the app if you have problems with light flickering. Tap the toggle
  • Forståelse af reguleringstilstandsprioritet

    Wiser Home – Systembrugervejledning (Danmark)

  • Resetting the device

    System M and System D - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    Resetting the device Resetting the device Resetting the device You can reset the Socket outlet to the factory default. It can be reset manually at any time, e.g., when the Hub is replaced. Short press the push button 3 times and hold for 10 seconds to reset the device to the factory default mode
  • Troubleshooting

    Wiser Home – System User Guide (Germany, Austria)

    Hub. After pressing 3 times, the device LED blinks amber for 30 s. Pairing mode has changed. Press the Reset button on the device 3 times then hold for 20 s, until the LED blinks red. The device should reboot into the correct mode. The hub is not communicating or receiving updates. IPv4 is not
  • Troubleshooting

    Wiser Home – System User Guide (Denmark)

    Hub. After pressing 3 times, the device LED blinks amber for 30 s. Pairing mode has changed. Press the Reset button on the device 3 times then hold for 20 s, until the LED blinks red. The device should reboot into the correct mode. The hub is not communicating or receiving updates. IPv4 is not
Page 112 of 163