DUG_SysM/SysD SSO 16 A_WH-07

Resetting the device

You can reset the Socket outlet to the factory default. It can be reset manually at any time, e.g., when the Hub is replaced.

  1. Short press the push button 3 times and hold for 10 seconds to reset the device to the factory default mode.

  2. After 10 s, LED starts blinking red then release the push button.

    The LED stops blinking upon successful reset of the device.

The plug restarts and blinks green for a few seconds.
NOTE: All configuration data, user data and network data are deleted.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?