Showing 1,201 - 1,210 of 1,449 results

Page 121 of 145
  • Wiser Hub 2nd Generation

    Wiser Home – System User Guide (UK, Ireland)

    latest version, you will be prompted to update before proceeding with the setup. Put the Hub into setup-mode as per the instruction provided by the app. Then tap Next (A). Connect your smartphone to the Hub’s temporary Wi-Fi ® network either by QR Code connection or Manual connection. If you cannot
  • Wiser Hub 2nd Generation

    Wiser Home – System User Guide (Germany, Austria)

    latest version, you will be prompted to update before proceeding with the setup. Put the Hub into setup-mode as per the instruction provided by the app. Then tap Next (A). Connect your smartphone to the Hub’s temporary Wi-Fi ® network either by QR Code connection or Manual connection. If you cannot find
  • Création d’un automatisme

    Odace - Thermostat connecté filaire 2 A – Guide de l'utilisateur de l’appareil Wiser Home

    sélectionnez l'une des options suivantes : Changement d’état d’un équipement (sélectionnez l’équipement) Mode Absence (activez ou désactivez) Un maximum de 10 conditions peuvent être ajoutées. Pour supprimer une condition ajoutée, balayez vers la gauche et appuyez sur (D). Afin de régler un horaire
  • Création d’un automatisme

    Micromodule chauffage électrique FIP – Guide de l'utilisateur de l’appareil Wiser Home

    condition : Une des conditions doit être remplie pour déclencher un automatisme. Appuyez sur Ajouter des conditions (C) et sélectionnez l’une des options suivantes (D) : Changement d’état d’un équipement (sélectionnez l’appareil) Mode Absence (activez ou désactivez) Changements de prix de l’énergie
  • Room setting

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    between a room being occupied and then transitioning to an unoccupied state.This delay ensures that the system doesn't immediately switch to an unoccupied mode when a room becomes vacant, preventing unnecessary fluctuations and providing a grace period in case the room becomes occupied again
  • Assigning a light group to the Wireless switch

    LK FUGA Wiser wireless battery 4 button switch – Wiser Home Device User Guide

    tap Save. If the device is in sleep mode, press the top-left push button on the Wireless switch 3 times to wake up the device. Then tap Confirm in the app to apply the settings. For more information, refer to Wake up the device. Each group can include up to 60 devices. You can create a maximum of 20
  • Room setting

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    between a room being occupied and then transitioning to an unoccupied state.This delay ensures that the system doesn't immediately switch to an unoccupied mode when a room becomes vacant, preventing unnecessary fluctuations and providing a grace period in case the room becomes occupied again
  • Wiser Hub 2nd Generation

    Wiser Home – System User Guide (Spain and Portugal)

    latest version, you will be prompted to update before proceeding with the setup. Put the Hub into setup-mode as per the instruction provided by the app. Then tap Next (A). Connect your smartphone to the Hub’s temporary Wi-Fi ® network either by QR Code connection or Manual connection. If you cannot find
  • Room setting

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    between a room being occupied and then transitioning to an unoccupied state.his delay ensures that the system doesn't immediately switch to an unoccupied mode when a room becomes vacant, preventing unnecessary fluctuations and providing a grace period in case the room becomes occupied again shortly
  • Setting Tariff

    Wiser Home – System User Guide (Sweden, Finland)

    change charging mode from Wiser Home AI to Charge Now or Manual or Customized Schedule. Feed in tariff: Feed in tariff will be shown only if you have set the PowerTag for Solar or Solar and Battery which feed electricity to the Grid.The electricity generated from solar or solar and battery that is
Page 121 of 145