SUG_SV_FI_WH-04

Setting Tariff

You can set tariff in the Wiser Home app to access your energy cost and billing data.

The Tariff option available only if you have installed the following energy monitoring device installed at your home.

  • EVlink Home Smart

  • Schneider Charge

  • Wiser Power Micromodule

  • Connected Sockets

  • PowerTag Energy

  • Wiser Plug

You can set the tariff based on your contract type:

  • Flat rate: The fixed rate for the entire time period of electricity service. Configuring - flat rate.

    Peak/Off-Peak Hours rate: Peak rate is the rate set to a specific period of time at which electrical consumption is at its highest. Off peak rate is the time period when the demand for power is at its lowest. You pay for each unit of electricity consumed for the time period set. Refer to Configuring - peak rate.

    Dynamic Tariff: In dynamic tariff, the prices vary hour by hour based on real-time market conditions, helping you save when demand is low. Refer to Dynamic Tariff.

  • None Electricity rate is not set, no information related to bill will be shown in the app.

    NOTE:
    • By default, No Contract option is set.

    • Before changing your tariff type from peak rate or flat rate to no contract, please change charging mode from Wiser Home AI to Charge Now or Manual or Customized Schedule.

  • Feed in tariff:

    IMPORTANT: Feed in tariff will be shown only if you have set the PowerTag for Solar or Solar and Battery which feed electricity to the Grid.
    The electricity generated from solar or solar and battery that is not used is exported to the electricity grid. You are eligible for a payment for the exported electricity. This payment is called a feed-in tariff.

    Refer to Configuring - feed in tariff.
    NOTE: You can see the tariff data based on your local currency.

Once the device is commissioned, you will get notified that this feature is available. The Tariff Entry screen appears on the Home screen.

  1. Tap Continue.

  2. Read the feature update and swipe to navigate to next screen.

  3. Tap to close the overlay screen.

    NOTE: If you have not configured your tariff, a push notification will be sent after 2 weeks and the last reminder after 6 weeks.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?