Showing 1,251 - 1,260 of 1,622 results

Page 126 of 163
  • Exxact - Connected Motion Sensor with Push-button Dimmer LED Wiser Home Device user guide

    /Dimming the device manually ...............................................18Turning On/Off device using app ..........................................................19Adjusting the brightness level using app ...............................................19Away Mode
  • Unica - Connected Wireless Switch 1-gang/2-gang Wiser Home Device user guide

    DUG_Unica-Wireless Switch_WH-05 37 Unica- Connected Wireless Switch 1-gang/2-gang Select Moment Select Moment Please select the Moment you want toassign to the top right gang switch. Away Mode Boost All Cancel all overrides Bienvenue Balcony Movie night Top Right Bottom Left Bottom Right Movie
  • Unica - Variateur rotatif universel connecté Guide de l'utilisateur de l'appareil domestique Wiser

    Appuyez brièvement 5 fois de suite rapidementsur le bouton-poussoir. Le voyant clignote en vert une foispar seconde. Le mode d’appairage est actif pendant60 secondes. Lorsque l’appairage est terminé, levoyant arrête de clignoter. Dépannage dans Quick Home Connect Symptôme Cause possible Solution La
  • Insights+

    Wiser Home – System User Guide (UK, Ireland)

    over past months. You can view savings in £ or kWh. It also displays savings from Away Mode and Eco Mode, with an option to enable Eco Mode for additional savings. How the weather affects your heating (F) This section shows how weather impacts your heating system's performance. We consider the
  • Pairing two Dimmers

    Wiser Multiwire Micro Module LED Dimmer – Wiser Home device user guide

    mechanical push-button. Refer to the below wiring diagram. You must put both dimmers in a pairing mode at the same time. The pairing mode will be active for about a minute. HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH Safe electrical installation must be carried out only by skilled professionals
  • Creating an automation

    PowerTag Control – Device user guide

    based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): The Away Mode is intended to set your Home to a practical state for longer absences, such as leaving for the weekend. Maximum 10 conditions can be added. Select a
  • Heat report

    Wiser Home – System User Guide (Denmark)

    the set temperature; the black line shows the set (target) temperature, i.e. Wiser’s heating schedule for the room (if in Auto mode) or the manually selected set temperature (if in Manual mode). This line indicates the room temperature that Wiser is regulating to at all times. The Single room view
  • Configuring the device

    Unica - Connected Motion Sensor with Dimmer LED – Wiser Home Device user guide

    the name of the device. B Location: Tap to assign the device to any room (such as living room, bedroom, kitchen etc). For more information, refer to Setting the device location. C RL-LED Mode: You can improve the dimming quality in the app if you have problems with light flickering. Tap the toggle
  • LK FUGA® Wiser wireless PIR dimmer with neutral Wiser Home Device user guide

    ..........................................................20Adjusting the brightness level using app ...............................................20Away Mode ........................................................................................21Voice control
  • Appairage de deux variateurs

    Wiser micromodule multifilaire pour variateur LED – Guide d'utilisation de l'appareil Wiser Home

    Connect. Un ou plusieurs variateurs doivent être raccordés à un bouton-poussoir mécanique double. Reportez-vous au schéma de câblage ci-dessous. Vous devez placer les deux variateurs en mode d’appairage en même temps. Le mode d’appairage reste actif pendant environ une minute. RISQUE DE DÉCHARGE
Page 126 of 163