DUG_Multiwire Puck Dimmer_WH–04

Pairing two Dimmers

You can pair 2 dimmers as a part of Quick Home Connect for wireless home automation.
NOTE:
  • You can operate 2 dimmers without the need for Wireless switch as a part of Quick Home Connect.

  • One or more dimmers should be connected to a 2 gang mechanical push-button. Refer to the below wiring diagram.

  • You must put both dimmers in a pairing mode at the same time. The pairing mode will be active for about a minute.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Safe electrical installation must be carried out only by skilled professionals. Skilled professionals must prove profound knowledge in the following areas:
- Connecting to installation networks.
- Connecting several electrical devices.
- Laying electric cables.
- Safety standards, local wiring rules and regulations.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK
- Make sure that the terminal connection area does not come in contact with the metallic parts of any device installed in the same location.
- Do not short the outputs to neutral.
Failure to follow these instructions will result in death or serious injury.
Below are 2 scenarios where you can pair the dimmers with each other.

Scenario 1: Dimmer–1 is wired to a 2 gang mechanical push-button and Dimmer–2 is not connected to any push-button and it remotely controlled by Dimmer–1.
Upon pairing, you can control the Dimmer–2 from Dimmer–1.


  1. On Dimmer–1, short press the right mechanical push button 5 times in quick succession.

  2. On Dimmer–2, short press the Setup/Reset button 5 times in quick succession on the dimmer.

The status LED blinks green on the dimmer LED.
NOTE: If the dimmer is located behind the mechanical push-button, the status LED is not visible.

The light connected to the dimmer blinks for a few times. The dimmer can now be controlled by the push-button.

Operating the dimmers: Short press the push buttons to turn on/off the light as mentioned in the following table.
Push button control Load
Left push button (Wired to terminal 1) Light 1
Right push button (Wired to terminal 2) Light 2
  • Press and hold the push button to adjust the brightness of the light.

    NOTE: This step is same for both the (right and left) push-buttons.


Scenario 2: Both dimmers are wired to their respective push-buttons.
Upon pairing, both the dimmers can be controlled vice versa. That means Dimmer–1 can control Dimmer–2 and Dimmer–2 can control Dimmer–1.


  1. On Dimmer–2, short press the right mechanical push button 5 times in quick succession.

  2. On Dimmer–1, short press the Setup/Reset button 5 times in quick succession on the dimmer.

The light connected to the dimmer blinks for a few times. The dimmer can now be controlled by the mechanical push-button.


Operating the dimmers: Short press the push buttons to turn on/off the light as mentioned in the following table.
Push button control Load
Dimmer 1
Left push button (Wired to terminal 1) Light 1
Right push button (Wired to terminal 2) Light 2
Dimmer 2
Left push button (Wired to terminal 1) Light 2
Right push button (Wired to terminal 2) Light 1
  • Press and hold the push button to adjust the brightness of the light.

    NOTE: This step is same for both the (right and left) push-buttons.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?