Showing 1,261 - 1,270 of 1,648 results

Page 127 of 165
  • LK FUGA® - Wiser wireless socket outlet 1½ M Wiser Home Device user guide

    consumption of thesystem below the established limit. This limit is determined by your contractspecifications, so it's important to refer to the Setting Tariff section for informationon peak and off-peak rates. Eligible devices will be automatically incorporated intothe Anti-Tripping Management system
  • About the device

    Wiser Micro Module Light Switch – Wiser Home Device user guide

    connected device that can be controlled from the switch or through the Wiser app. It can switch ohmic, inductive or capacitive loads. Do not control any devices that depend on a permanent power supply. Additional features: Remote controlled with maximum of 10 mechanical push-buttons. Setting a time schedule via Wiser Home app.
  • Home Screen Settings

    Wiser Home – System User Guide (Denmark)

    Home Screen Settings Home Screen Settings Home Screen Settings The Wiser Home App offers options to customize the Home Screen. Find the Home Screen options in the Settings Menu. Setting ON OFF Start on Control Tab The App opens directly in the Control tab. The App will open on the Home Screen. Show
  • Home Screen Settings

    Wiser Home – System User Guide (UK, Ireland)

    Home Screen Settings Home Screen Settings Home Screen Settings The Wiser Home App offers options to customise the Home Screen. Find the Home Screen options in the Settings Menu. Setting ON OFF Start on Control Tab The App opens directly in the Control tab. The App will open on the Home Screen. Show
  • Wiser-älypistoke 16 A Wiser Home -laitteen käyttöopas

    ansiosta käyttäjät voivat hallita PCM:n valvomiakuormia entistä paremmin. Voit rekisteröidä enintään kahdeksan kuormaakerrallaan, mikä auttaa pitämään järjestelmän kokonaiskulutuksen alle asetetunrajan. Tämä raja määräytyy sopimustesi eritelmien mukaan, joten on tärkeäätutustua Setting Tariff
  • Pairing the device with the Wiser Hub

    Unica - Connected Blind Control Switch – Wiser Home Device user guide

    Device Type: Shutter: Proceed to step 8. Shutter with tilting slats: Proceed to step 9 to 11. Tap Shutter Next and enter the open/close duration of shutter. Refer to Setting default run time. Tap Shutter with tilting slats Slat Type , select a slat type and tap Set: Horizontal Tilted Vertical Tap
  • Checking the device history

    Wiser Window/Door Sensor – Wiser Home Device user guide

    , the window or door events will not appear in the history. On the Control tab, tap All devices or a room tab where the sensor is located. On the device control panel page, tap History. The history page displays all logged-in events, even if the sensor notification toggle switch is disabled. For more information about sensor notification toggle switch, refer to Setting device notification.
  • Unica - Connected Blind Control Switch

    (0) 1 41 29 70 00 Configuring the device Configuring the device Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison - France + 33 (0) 1 41 29 70 00 Setting the device location Setting the
  • Configuring the device

    Wiser Radiator Thermostat – Wiser Home Device user guide

    16A), or Temperature & Humidity Sensor), the system calculates the average temperature measured from all devices to control the heating based on the overall room temperature. If several Radiator Thermostats are installed in a room, the system uses the average temperature of all Radiator Thermostats.For more details, refer to the Setting the device as temperature source.
  • Using the device

    Odace - Connected Multiwire Universal Push-button Dimmer LED – Wiser Home Device user guide

    increase/decrease the brightness of your dimmer. For more information, refer to Adjusting the brightness. B Tap to turn the device on/off. C Tap to open the Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule. D Tap to add the device to the Favourite
Page 127 of 165