DUG_Radiator Thermostat_WH-07

Configuring the device

IMPORTANT: The temperature data from the Radiator Thermostat sensor will be used as an input for the room’s heating system. If a room has an additional temperature measuring device (such as a Room Thermostat, Connected Thermostat (2A or 16A), or Temperature & Humidity Sensor), the system uses that device for temperature measurement because it is typically placed in a more representative location than the radiator thermostat. Finally, if a room has multiple temperature measuring devices (Room Thermostat, Connected Thermostat (2A or 16A), or Temperature & Humidity Sensor), the system calculates the average temperature measured from all devices to control the heating based on the overall room temperature.
  • If several Radiator Thermostats are installed in a room, the system uses the average temperature of all Radiator Thermostats.

For more details, refer to the Setting the device as temperature source.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?