DUG_Window/Door Sensor_WH-06

Checking the device history

Using the Wiser Home app, you can view the sensor history, which provides information about when the window/door was open. The sensor records each event and stores it in the cloud.
NOTE: If the cloud connection is lost, the window or door events will not appear in the history.
  1. On the Control tab, tap All devices or a room tab where the sensor is located.
  2. On the device control panel page, tap History.
    TIP: The history page displays all logged-in events, even if the sensor notification toggle switch is disabled. For more information about sensor notification toggle switch, refer to Setting device notification.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?