DUG_Micro Module Light Switch_WH-07

About the device

The Wiser Micro Module Light Switch (hereinafter referred to as Puck Switch / Micro Module Switch) combines the advantages of smart switch functionality with ordinary mechanical push-button switches. It transforms a conventional switch into a connected device that can be controlled from the switch or through the Wiser app. It can switch ohmic, inductive or capacitive loads.
NOTE: Do not control any devices that depend on a permanent power supply.

Additional features:

  • Remote controlled with maximum of 10 mechanical push-buttons.

  • Setting a time schedule via Wiser Home app.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?