Showing 1,341 - 1,350 of 1,648 results

Page 135 of 165
  • Ovalis - Connected Single Socket Outlet 16 A Wiser Home Device user guide

    set by your Contract limit, refer to Setting Tariff. Devicesthat are eligible will be added automatically to the Anti-Tripping Management. IMPORTANT: When a device is managed by the Anti-Tripping management,the Schedules, Moments and Automations for that device are not executed.NOTE: Maximum of 8
  • LED Indications

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    pressing " O" and " +" for 2 s to enter advanced settings menu In advance setting menu the thermostat matrix display flashes " P1" or " P2... P9" when +/– button is pressed. Note: When + button is pressed, preset increases by one; similarly, the preset decreases by one when the – button is pressed. For
  • Exxact - Connected Thermostat Room/Floor 16 A Wiser Home Device User Guide

    ..............................................................22Advanced device settings ....................................................................23Floor sensors settings .........................................................................26Room setting
  • Creating a moment

    PowerTag Control – Device user guide

    the Add actions menu, you can select the devices (C). Once the device are selected, tap Done. On the Moment creator page, tap on the device to set the preferred action (to turn on/off) and then tap Set on the upper right corner. After setting all actions, tap Save. Once the moment is saved, it will
  • Creating a moment

    LK® One Wiser Motion Sensor with Switch 10A – Wiser Home Device user guide

    actions menu, you can select the devices (C). Once devices are selected, tap Done. On the Moment creator page, tap the device to set the condition. For example, if it is a Motion Sensor Switch: Tap to turn on (D) and tap Set on the top-right screen. After setting all conditions, tap Save. Once the
  • LED indications

    Exxact - Connected Double Socket Outlet 16A – Wiser Home Device user guide

    . Setting (Default state) LED Indication Description The Red LED glows. The Red LED glows when the output is switched ON. All the LEDs are OFF. The LEDs are OFF, when the output is OFF. Alarms LED Indication Description Blinking red fast When there is an overload or over-temperature alarm and the device is switched off. Refer to the Troubleshooting to clear the alarms.
  • ARGUS Motion Sensor Outdoor 360 Wiser Home Device user guide

    sensor usinga screwdriver. Time setting Time setting: Adjusts the duration for which the sensor activates or triggers the connected load afterdetecting motion. NOTE: If you re-trigger the sensor, the timer will get reset. You can also change the status of the loadbefore the set time expires. For more
  • Wiser HubR 2nd Generation

    Wiser Home – System User Guide (UK, Ireland)

  • Example of an automation

    Sensor de temperatura/humedad Wiser – Guía del usuario del dispositivo Wiser Home

    Example of an automation Example of an automation Example of an automation This demonstration guides you through setting up an automation that activates heating to a set temperature of 20 °C when the room temperature drops below 18 °C. To ensure proper heating control, you must create two separate
  • Example of an automation

    Wiser-lämpötila-/kosteusmittari – Wiser Home -laitteen käyttöopas

    Example of an automation Example of an automation Example of an automation This demonstration guides you through setting up an automation that activates heating to a set temperature of 20 °C when the room temperature drops below 18 °C. To ensure proper heating control, you must create two separate
Page 135 of 165