DUG_Temperature/Humidity Sensor_WH-06

Example of an automation

This demonstration shows you how to create an automation to turn on the Heating to the desired temperature (set point) of 20° C when the temperature is less than 18° C.
HUOMAUTUS: It is mandatory to create two automations:
  • First, switch on the heater at the desired 20° C when the room temperature is 18° C or lower.

  • Second, switch off the heater when the room temperature is at 25° C or above.


The room heater will not turn off automatically until you create another automation.
  1. Go to Automation > to create an automation.
  2. To add a condition, tap Add Condition > Device status change > Temperature/Humidity Sensor > Temperature.
  3. Set the temperature as 18° C (A) and the condition as less than (B) and tap Set.
  4. Read the information and tap OK.
  5. To add an action, tap Then > Add an action > Control a device > Heating > Setpoint. Set the temperature to 20° C (C), then tap Set.
  6. Read the information and tap OK.
  7. Enter the name of the automation.
    EHDOTUS: You can choose the cover image that represents your automation by tapping .
  8. Tap Save.
    Once the automation is saved, it is visible on the Automation tab.
    HUOMAUTUS: You can enable or disable saved automations on the Automations tab by using (D).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Auttoiko tämä?