DUG_PTC_WH-03

Creating a moment

  1. On the Home screen, tap Automations .
  2. Go to Moments and tap to create a moment.
  3. Enter the name of the moment (A).
    TIP: You can choose the cover image that represents your moment by tapping .
  4. Tap Add actions (B) to select the list of devices.
  5. In the Add actions menu, you can select the devices (C).
  6. Once the device are selected, tap Done.
  7. On the Moment creator page, tap on the device to set the preferred action (to turn on/off) and then tap Set on the upper right corner.
  8. After setting all actions, tap Save.
    Once the moment is saved, it will appear on the Moments tab. Tap on the moment to enable it.

    TIP:

    • If you want to see the created moments on the Home screen, go to Home > > Home Screen > Moments. Enable the toggle button to view moments on the Home screen.

    • You can also rearrange the moments by tapping Edit from the Moments tab on the Home screen, or by tapping Automation > Moments > Reorder.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?