Showing 1,451 - 1,460 of 1,648 results

Page 146 of 165
  • System M and System D - Connected Push-button Module, 1-gang/2-gang Wiser Home Device user guide

    Next and enter the following durations: a. Open duration: Time taken to open the shutter. b. Close duration: Time taken to close the shutter. c. Tilt duration: Time taken to rotate the slats completely from closed toopen position.Refer to Setting default run time, page 32. 10. Tap Submit.After you
  • Wiser Multiwire Micro Module LED Dimmer Wiser Home device user guide

    ..............................................................19Configuring the device ..............................................................................21 Setting the device location ...................................................................23Setting Dimming Mode
  • eSetup App

    Wiser Home – System User Guide (Germany, Austria)

    individual Devices. You can test the Devices. To configure a Device: Choose the Device type (Light and Shutter Devices). Choose the specific Device type, e.g. rotary dimmer. Connect the Device to the app by setting it into pairing mode. The app will show you how to set the Device into pairing mode. Set the Name for the Device. Assign the Device to a Room. Test the Device.
  • Exxact - Connected Single Socket Outlet 16 A

    70 00 www.se.com Setting the device location in the room Setting the device location in the room Using the Wiser Home app, you can assign your Socket outlet to any room (such as bedroom, living room, dining room etc.). Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41
  • System M y Sistema D - Toma de corriente inteligente, 1 elemento, 16 A Guía del usuario del dispositivo Wiser Home

    PowerTag nocoincide con la tarifa. Consulte Setting Tariff. • Empareje los dispositivos compatibles. Consulte el emparejamiento deldispositivo (en función de los dispositivos que tenga instalados): micromódulode potencia, enchufe de EV, enchufe inalámbrico, enchufe conectado, EVlinkHome Smart, Schneider
  • Device presetting

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    /Oil Boiler 20 Off P2 Hydronic Radiator/Gas Boiler 10 Off P3 Hydronic Underfloor 10 On *Cycle time:: This setting determines the length of each on/off cycle of the output relay. The percentage of time within that cycle time that the relay is on is varied based on demand. A longer cycle time may be more
  • LED indications

    Mureva EVlink – Wiser Home Device User Guide

    the device User Action LED Indication Status Press the push button 3 times and hold it down once for > 10 s. After 10 s, the LED starts blinking red. The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts and LED is off after reset. Setting
  • Climate control

    Wiser Home – System User Guide (UK, Ireland)

    be available. H Add or remove the device from Favourite devices. Refer to Managing Favourites J Navigate to the Room Details of the room to which the climate control is assigned. Setting up a Climate Control While setting up your Climate Control, make sure to consider the following information
  • Device presetting

    Wiser Flush-mounted Thermostat 2 A – Wiser Home Device user guide

    Heat Pump/Oil Boiler 20 Off P2 Hydronic Radiator/Gas Boiler 10 Off P3 Hydronic Underfloor 10 On You can also enable/disable valve protection in Wiser app. Refer valve protection settings. *Cycle time: This setting determines the length of each on/off cycle of the output relay. The percentage of
  • Device Details

    Wiser Home – System User Guide (Sweden, Finland)

    Device Details Device Details Device Details You can find all relevant settings of a Device in the Device details. You can navigate to the Device details from the List of Devices by tapping the Device or from the Device control by tapping the device setting. A Tap to change the name of the device
Page 146 of 165