SUG_SV_FI_WH-04

Device Details

You can find all relevant settings of a Device in the Device details.

You can navigate to the Device details from the List of Devices by tapping the Device or from the Device control by tapping the device setting.

A

Tap to change the name of the device.

B

Tap to change the location of the of the device

NOTE:
  • A Device can only be assigned to one Room.

  • Devices (except the Climate devices) which you remove from the room are listed as unassigned.

  • Climate Devices must be assigned to a Room in order to function. Climate Devices will combine into a single Climate Control when assigned to the same room. You can find detailed information about the Climate Control in chapter: Climate Control.

C

Tap to identify the device.

NOTE: Most of the devices will light up their status LED to help locate them. You can find the detailed information about this behavior in the Device User Guide of the respective device. Refer to List of Wiser Devices for the links to Device user guide for each devices.

D

Tap to remove the device from the Wiser system.

NOTE: Removing a device should only be necessary if it needs to be replaced or as part of troubleshooting, for example, if you need to reconnect the device to the hub.

E

The battery charge level indicator which displays the current battery status for battery-powered devices.

G

Zigbee Signal strength indicator which displays the current signal strength of the zigbee devices. Refer to About Signal Strength to know more about the zigbee signal strength.

NOTE: This feature is not applicable for Wiser Plug device.
IMPORTANT: The signal strength is not displayed for Wi-Fi® devices (expect for Hubs). It will only display no-signal () if the device is offline.

Some devices have specific features and settings. For example, Shutter devices have an option to set the duration for opening and closing. You can find detailed information in the Device User Guide of the respective device. Refer to List of Wiser Devices for the link to device user guide of each devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.