System User Guide Wiser Home (Germany, Austria) - 14

eSetup App

eSetup for Electricians App is the dedicated app for Electricians to configure Smart Home and Smart panel devices.

No need for PC or complex tools to configure smart systems – everything can be done via smartphone, thanks to eSetup for Electricians App

With eSetup for Electricians App you can,

  • Commissioning of Wiser products with step by step guidance

  • See the complete installation in DEMO Mode (no need of actual devices)

  • Define the system and settings of the devices

  • Verify and test the installation

Get connected to Bluetooth or Wifi to the product directly. This dedicated application for Electricians is a commissioning tool for Wiser devices in residential and SmartLink, Powertag devices in Small Buildings.

NOTE: Not all the wiser devices can be configured using the eSetup app. The app offer the configuration for devices such as Light and Shutter Devices, Evlink Home Smart / Schneider Charge.

Using the eSetup app

With the eSetup app, you can configure Devices without the need of an internet connection.

Your smartphone will connect to the Device directly.

You can set the Name of the Device and assign it to a Room. Other settings are depending on the individual Devices.

You can test the Devices.

To configure a Device:

  1. Choose the Device type (Light and Shutter Devices).

  2. Choose the specific Device type, e.g. rotary dimmer.

  3. Connect the Device to the app by setting it into pairing mode.

    The app will show you how to set the Device into pairing mode.

  4. Set the Name for the Device.

  5. Assign the Device to a Room.

  6. Test the Device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.