Showing 291 - 300 of 1,648 results

Page 30 of 165
  • Setting up a schedule

    Ovalis - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule Using the Wiser Home app, you can create or assign a schedule to the Socket outlet. On the Home screen, tap . Go to Schedule tab, tap . Enter the Schedule name and select Appliances from the TYPE menu. Select the Smart Socket Outlet
  • Setting heat source type

      Same topic found multiple times in this document:
    Setting heat source type Using the Wiser Home app, you can set the heat source type such as Gas Boiler, Oil Boiler, Electric Boiler, or Heat Pump. Heat source type only required for relay channel.To set the heat source type. On the Home screen, tap . Tap Devices Boiler Relay Heat Source Type (A) to select given option: Gas Boiler (Default) Oil Boiler Electric Boiler Heat Pump
  • Setting the device location

    Wiser Window/Door Sensor – Wiser Home Device user guide

    Setting the device location Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). On the Home screen, tap . Tap Devices, select the device from the list for which you wish to change the location. Tap Location to
  • Setting up the Hub

    Wiser Home – System User Guide (Germany, Austria)

    Setting up the Hub Setting up the Hub Setting up the Hub In order to be able to control the system via your smartphone, the hub must be connected to the internet. You can set up the Hub by using the app as Home Owner and Professional Installer. The app offers the Professional Installer menu for
  • Setting up a schedule

    Odace - Connected Relay Switch 10 A – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule The relay switch can be fully controlled by a schedule. Once the schedule is set, the relay switch operates at a given time. On the Home screen, tap . Go to Schedules and tap to create a schedule. Enter the name of the schedule (A
  • Setting the device location

    Unica - Connected Blind Control Switch – Wiser Home Device user guide

    Setting the device location Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). On the Home screen, tap . Tap Devices, select the device from the list for which you wish to change the location. Tap Location to
  • Setting boost mode manually

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    Setting boost mode manually Setting boost mode manually Setting boost mode manually You can enable and disable boost mode manually.When enabled the temperature increases by 2° C for temperature control modes and by +2 over the setpoint. To enable boost mode: Press the rotary push-button until the
  • Setting up a schedule

    PowerTag Control – Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule The control device can be fully controlled by a schedule. Once the schedule is set, the device operates at a given time. On the Home screen, tap Automations . Go to Schedules and tap to create a schedule. Enter the name of the
  • Setting up the Hub

    Wiser Home – System User Guide (Belgium)

    Setting up the Hub Setting up the Hub Setting up the Hub In order to be able to control the system via your smartphone, the hub must be connected to the internet. You can set up the Hub by using the app as Home Owner and Professional Installer. The app offers the Professional Installer menu for
  • Setting the device location

    Exxact - Connected Multiwire Universal Rotary Dimmer LED – Wiser Home Device user guide

    Setting the device location Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). On the Home screen, tap . Tap Devices, select the device from the list for which you wish to change the location. Tap Location to
Page 30 of 165