DUG_Boiler Relay_WH–05

Setting heat source type

Using the Wiser Home app, you can set the heat source type such as Gas Boiler, Oil Boiler, Electric Boiler, or Heat Pump.
NOTE: Heat source type only required for relay channel.
To set the heat source type.
  1. On the Home screen, tap .
  2. Tap Devices > Boiler Relay > Heat Source Type (A) to select given option:
    • Gas Boiler (Default)
    • Oil Boiler
    • Electric Boiler
    • Heat Pump
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?