SUG_NL_WH-04

Setting up the Hub

In order to be able to control the system via your smartphone, the hub
must be connected to the internet.

You can set up the Hub

by using the app as Home Owner and Professional Installer.

The app offers the Professional Installer menu for setting up a Wiser System and adding devices without having to be logged in.

You can also setup the Wiser System by using the app as a Home Owner after creating an account. Refer to Setting up an Account for information on how to create an account.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.