DUG_SysM - Connected Thermostat 2 A, ZB_WH-07

Setting boost mode manually

You can enable and disable boost mode manually.
When enabled the temperature increases by 2° C for temperature control modes and by +2 over the setpoint.

To enable boost mode:

  1. Press the rotary push-button until the display flashes (press 2 times if the device is in standby mode, 1 time if the setpoint is already displayed).

  2. Press the rotary push-button once to enter boost menu.


    +1 flashes on thermostat matrix.
    NOTE: The thermostat will exit boost mode if there is no interaction within 5 seconds after pressing rotary push-button.
  3. Press the rotary push-button to navigate between the boost hours from +1 to +3

    NOTE: When you press the rotary push-button on the device, the boost mode selection cycle through +1+2+3- - (boost cancel) and again back to +1.

    After selecting the boost hours, thermostat will save and exit boost mode if there is no interaction within 5 s.

For example:
If current setpoint is 12° C and you enable boost mode by selecting +3.
The boost mode will set the setpoint temperature to 14° C for next 3 hour. After 3 hour setpoint will return to 12° C.


To disable boost mode:

  1. Press the rotary push-button once.
    +1 flashes on thermostat matrix.

  2. Turn the rotary push-button clockwise button for thermostat to display – – (boost cancel).

    After selecting the boost cancel, thermostat will save and exit boost mode if there is no interaction within 5 s.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?