Showing 3,181 - 3,190 of 9,859 results

Page 319 of 986
  • Energy

    Wiser Home – System User Guide (France)

    Energy Energy Energy PowerLogic TM - PowerTag Resi9 M63 R9M20 R9M21 R9M22 R9M40 R9M43 R9M41 R9M42 It is a compact, robust, and easy-to-install Class 1 wireless communication energy sensor. It is used together with the Wiser Hub to collect information from every equipped circuit to measure how much
  • Configuring UFH actuator

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    temperature.The thermostat can also be used as a temperature sensor and a temperature set point selector for other heating devices like 16A Relay or ELKO - Smart Radiator Thermostat. Refer, pairing the device. Refer, . Assign a room to the thermostat once it has been paired and then tap Next to configure
  • Configuring UFH actuator

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    temperature.The thermostat can also be used as a temperature sensor and a temperature set point selector for other heating devices like 16A Relay or Connected Thermostat (2A or 16A). Refer, pairing the device. Assign a room to the thermostat once it has been paired and then tap Next to configure UFH. Tap
  • Unica - regulador LED universal de pulsación conectado Guía del usuario del dispositivo Wiser Home

    ://www.se.com Información legalLa información proporcionada en este documento contiene descripciones generales,características técnicas o recomendaciones relacionadas con productos osoluciones. Este documento no pretende sustituir a un estudio detallado o un plan de desarrollo oesquemático específico de
  • Acerca do documento

    Micromódulo Interruptor Wiser – Guia do utilizador do dispositivo Wiser Home

    características dos produtos descritos neste documento destinam-se a corresponder às características disponíveis em www.se.com. Como parte da nossa estratégia empresarial de melhoria constante, podemos rever o conteúdo ao longo do tempo para aumentar a clareza e a exatidão Se se verificar uma diferença
  • Caractéristiques techniques

    Schneider Charge – Guide de l'utilisateur de l’appareil Wiser Home

    Montage mural Tension nominale d’alimentation 400 V AC (+/- 10%) 50/60 Hz 3-ph 230 V AC (+/- 10%) 50/60 Hz 1-ph Puissance de sortie nominale 11 kW 16 A (3 P + N) 7,4 kW 32 A (1 P + N) 22 kW 32 A (3 P + N) Raccordement Câblage par le haut, l’arrière ou le bas Protection intégrée Filtre CC 6 mA RCD-DD
  • Managing shutter operation without temperature sensor

    Ovalis - Connected Blind Control Switch – Wiser Home Device user guide

    Managing shutter operation without temperature sensor Managing shutter operation without temperature sensor Managing shutter operation without temperature sensor Using the Wiser Home app, you can manage the shutter operation of a room where no temperature sensor is installed. To define the
  • Einen Zeitplan bearbeiten

    Wiser Home – Systemhandbuch (Deutschland, Österreich)

    Einen Zeitplan bearbeiten Einen Zeitplan bearbeiten Einen Zeitplan bearbeiten Im Bildschirm „Zeitplan-Details“: Tippen Sie auf das Symbol (A), um den Namen des Zeitplans zu ändern. Wählen Sie die Geräte (B) aus, auf die sich der Zeitplan bezieht. Wählen Sie den Tag (C) aus, für den Sie Schaltzeiten
  • Managing shutter operation without temperature sensor

    Unica - Connected Blind Control Switch – Wiser Home Device user guide

    Managing shutter operation without temperature sensor Managing shutter operation without temperature sensor Managing shutter operation without temperature sensor Using the Wiser Home app, you can manage the shutter operation of a room where no temperature sensor is installed. To define the
  • Away Mode

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    Away Mode Away Mode Away Mode When Away Mode (A) is activated, all rooms will be set to the Away temperature (default 16 °C). It will show a checkmark in the “Automation” page when active. You can find it in the “Automation” menu by tapping the “Automation” tab at the bottom of the Home screen
Page 319 of 986