Configuring UFH actuator
The thermostat can also be used as a temperature sensor and a temperature set point selector for other heating devices like 16A Relay or Connected Thermostat (2A or 16A).
- Assign a room to the thermostat once it has been paired and then tap Next to configure UFH.
- Tap Output Device (A) for slide up menu and select the UFH (B) from the list which is connected to the thermostat.
- Tap on Channels (C) and select the channel which controls the room where thermostat is located.
- Enable toggle switch (D), if you want monitor the floor temperature
using UFH floor sensor.
NOTE:
-
To change the UFH channel room refer Assigning a channel to the room.
-
Only one UFH floor sensor can be assigned to a room if you want to update refer Setting Floor Sensor Location.
-
- Tap Submit.
The thermostat is now listed on the Control tab under the All and the specific room tabs.