Showing 3,301 - 3,310 of 9,859 results

Page 331 of 986
  • Pairing the device with the Wiser Hub

    Wiser Temperature/Humidity Sensor – Wiser Home Device user guide

    proceed to step 4. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options: (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are
  • Pairing the device with the Wiser Hub

    Wiser Smoke Alarm - Battery – Wiser Home Device user guide

    the smoke alarm. When multiple smoke alarms are paired with the same Wiser Hub, a 868 MHz radio frequency (RF) interconnection is automatically created between smoke alarms. Locate the power switch on the rear side of the smoke alarm. Use a screwdriver to turn the power switch to ON position. When
  • Pairing the device with the Wiser Hub

    Wiser Smoke Alarm - 230 V – Wiser Home Device user guide

    the smoke alarm. When multiple smoke alarms are paired with the same Wiser Hub, a radio frequency (RF) interconnection is automatically created between smoke alarms. Locate the power switch on the rear side of the smoke alarm. Use a screwdriver to turn the power switch to ON position. When the smoke
  • Schneider Charge

    - França +33 (0) 1 41 29 70 00 Sobre o documento Sobre o documento Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison França + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison - França +33 (0) 1 41 29 70 00 Schneider Charge Schneider Charge A
  • Example of an automation

    Wiser Flush-mounted Thermostat 2 A – Wiser Home Device user guide

    Example of an automation Example of an automation Example of an automation This demonstration guides you through setting up an automation that activates heating to a set temperature of 20 °C when the room temperature drops below 18 °C. To ensure proper heating control, you must create two separate
  • Configuring UFH actuator

    Wiser Flush-mounted Thermostat 2 A – Wiser Home Device user guide

    temperature.The thermostat can also be used as a temperature sensor and a temperature set point selector for other heating devices like 16A Relay or Wiser Radiator Thermostat. Refer, pairing the device. Assign a room to the thermostat once it has been paired and then tap Next to configure UFH. Tap Output
  • Modo ausente

    Termostato Empotrado Wiser 2 A – Guía del usuario del dispositivo Wiser Home

    Modo ausente Modo ausente Modo ausente Cuando se activa el Modo Ausente (A), todas las salas se ajustarán a la temperatura de ausencia (por defecto 16 °C). Mostrará una marca de verificación en la página «Automatización» cuando esté activo. Puede encontrar la función en el menú «Automatización
  • User Settings

    Wiser BMS – Building Management System – User Guide

    User Settings User Settings User Settings Allows you to change your regional and theme settings according to your preferences. Regional Settings Language (A) Allows you to select the preferred language for the interface, making it easier to navigate and understand the system. Date, time and number
  • Resetting the device

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    Resetting the device Resetting the device Resetting the device You can manually reset the thermostat to factory settings or perform a soft reset. To perform a Soft reset : Press and hold the O touch button for more than 20 seconds. The thermostat flashes Sr, indicating soft reset, and it is
  • Push-button Module

    System M and System D- Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    and the push-button module will stop blinking. When the push-button module is connected to the relay or dimmer insert, the connected light blinks for a few times. Similarly, if the push-button module is connected to the shutter insert, the shutter moves up and down for a few times. You can also use
Page 331 of 986