DUG_Exxact - ZB Thermostat 16 A_WH-01

Away Mode

Away Mode (A) sets all rooms to a default temperature (16  °C). It appears with a check mark in the Automation page when active and can be accessed from the Automation menu by tapping the Automation tab at the bottom of the Home screen.
Only rooms with setpoints higher than 16  °C will change. For example, a room set to 5 °C will remain unchanged.
Away Mode overrides Boost and schedules, but you can still manually adjust setpoints, boost individual rooms, or turn hot water ON.
When active, rooms and hot water display Away Mode values, and hot water will turn OFF if selected in the Away Mode screen. For more information on Away Mode, refer to the Away Mode topic in the respective System User Guide

NOTE: Current temperature is not shown while Away Mode is active.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?