Showing 3,311 - 3,320 of 9,859 results

Page 332 of 986
  • About the Document

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    About the Document About the Document About the Document Document Scope This document provides instructions for installing, configuring, and using the System M and System D Connected Thermostat 2 A with the Wiser Home system. It explains how to set presets, pair with the Wiser Hub, adjust
  • Emparelhar o módulo antidisparo com o Schneider Charge

    Schneider Charge – Guia do utilizador do dispositivo Wiser Home

    Emparelhar o módulo antidisparo com o Schneider Charge Emparelhar o módulo antidisparo com o Schneider Charge Emparelhar o módulo antidisparo com o Schneider Charge Pode emparelhar o Módulo antidisparo e o Schneider Charge entre si para evitar distúrbios entre os dois. Assegurar-se de que a
  • Pairing the device with the Wiser Hub

    LK FUGA® Wiser wireless double relay – Wiser Home Device User Guide

    Home app to access your camera. Then, scan the QR code located on the device. If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I
  • Sensor de movimiento Wiser Guía del usuario del dispositivo Wiser Home

    este documento contiene descripciones generales,características técnicas o recomendaciones relacionadas con productos osoluciones. Este documento no pretende sustituir a un estudio detallado o un plan de desarrollo oesquemático específico de operaciones o sitios. No debe usarse para determinar
  • Energy

    Wiser Home – System User Guide (Spain and Portugal)

    Energy Energy Energy PowerLogic TM - PowerTag Resi9 F63 R9M60 R9M70 Itis a compact, robust, and easy-to-install Class 1 wireless communication energy sensor. It is used together with theWiser Hubto collect information from every equipped circuit to measure how much energy is consumed in the circuit
  • Boost All

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    Boost All Boost All Boost All You can apply a +2 °C boost for 1 hour to all rooms in the system. This action does not affect hot water. Since it is a one-time action, you will find Boost All (A) under the Automation menu by tapping the Automations tab at the bottom of the Home screen.
  • Configuring - flat rate

    Wiser Home – System User Guide (France)

    the Home screen, tap Energy Management Tariff Electricity. Tap (A) and select Flat. Tap (B) to set the contract limit. contract limit is already set when pairing the main PowerTag as Grid. Refer to Pairing the main device. Select your contract limit (kVA/A/kW) size from the dropdown menu, then tap and
  • Example of an automation

    Wiser Flush-mounted Thermostat 2 A – Wiser Home Device user guide

    Example of an automation Example of an automation Example of an automation This demonstration guides you through setting up an automation that activates heating to a set temperature of 20 °C when the room temperature drops below 18 °C. To ensure proper heating control, you must create two separate
  • Configuring UFH actuator

    Wiser Flush-mounted Thermostat 2 A – Wiser Home Device user guide

    temperature.The thermostat can also be used as a temperature sensor and a temperature set point selector for other heating devices like 16A Relay or Wiser Radiator Thermostat. Refer, pairing the device. Assign a room to the thermostat once it has been paired and then tap Next to configure UFH. Tap Output
  • Modo ausente

    Termostato Empotrado Wiser 2 A – Guía del usuario del dispositivo Wiser Home

    Modo ausente Modo ausente Modo ausente Cuando se activa el Modo Ausente (A), todas las salas se ajustarán a la temperatura de ausencia (por defecto 16 °C). Mostrará una marca de verificación en la página «Automatización» cuando esté activo. Puede encontrar la función en el menú «Automatización
Page 332 of 986