Showing 3,331 - 3,340 of 9,859 results

Page 334 of 986
  • Identificar o dispositivo

    Micromódulo Variador Wiser – Guia do utilizador do dispositivo Wiser Home

    Identificar o dispositivo Identificar o dispositivo Identificar o dispositivo Através da aplicação Wiser Home, identifique o relé entre os dispositivos disponíveis numa casa. No ecrã Inicial, toque em . Toque em Dispositivos Micromódulo variador Identificar (A). O LED de estado pisca a vermelho e
  • Identificar o dispositivo

    Sensor de fumo 230V Wiser – Guia do utilizador do dispositivo Wiser Home

    Identificar o dispositivo Identificar o dispositivo Identificar o dispositivo Através da aplicação Wiser Home, identifique o dispositivo entre os sensores de fumo disponíveis numa casa. No ecrã inicial, toque em . Toque em Dispositivos Identificar (A). O LED do sensor de fumo pode demorar até 60
  • Setting the device location

    Exxact – Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    Setting the device location Setting the device location Setting the device location You can add your Wireless Switch to any room (such as bedroom, living room, dining room etc.). To add a Wireless Switch to a room: On the Home screen, tap . Tap Devices 2-gang Connected Wireless Switch Location (A) to assign the Wireless Switch to an existing room or a new room (B) and tap Submit.
  • Pairing the device with the Wiser Hub

    Unica - Connected Relay Switch 10 A – Wiser Home Device user guide

    incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options: (A): Enter the MAC Address and Install Code, then tap Connect. The app will verify if the MAC address and Install code are valid. (B): Tap this option if you are unable to
  • Emparelhar um interruptor sem fios duplo com interruptor de controlo de estores duplo

    Unica - Comando de estores conectável – Guia do utilizador do dispositivo Wiser Home

    sequência rápida no interruptor sem fios. O LED de estado pisca a verde. Prima brevemente o primeiro interruptor de controlo de estores 5 vezes numa sequência rápida. O LED de estado pisca a verde. O estore subirá e descerá algumas vezes durante o processo de emparelhamento. O LED de estado para de
  • Room setting

    Wiser Flush-mounted Thermostat 2 A – Wiser Home Device user guide

    details. Unoccupied Offset: You set the setpoint when room is unoccupied. This helps to save energy by allowing the temperature to drift from the normal setpoint to a less comfortable but more energy-efficient level when the space is not in use. Occupied to Unoccupied Delay: You can set the time delay
  • Room setting

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    details. Unoccupied Offset: You set the setpoint when room is unoccupied. This helps to save energy by allowing the temperature to drift from the normal setpoint to a less comfortable but more energy-efficient level when the space is not in use. Occupied to Unoccupied Delay: You can set the time delay
  • About the Document

      Same topic found multiple times in this document:
    accuracy. If you see a difference between the characteristics in this document and the characteristics on www.se.com, consider www.se.com to contain the latest information. For your safety HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH Safe electrical installation must be carried out only by skilled
  • Room setting

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    details. Unoccupied Offset: You set the setpoint when room is unoccupied. This helps to save energy by allowing the temperature to drift from the normal setpoint to a less comfortable but more energy-efficient level when the space is not in use. Occupied to Unoccupied Delay: You can set the time delay
  • Pairing the Airzone device with the Wiser Hub

    Airzone Plenum and Aidoo Pro - Air conditioner – Wiser Home Device user guide

    Wiser Hub: The Wiser Hub and the Airzone devices should be updated to the latest system version. Both should be connected to the same Wi-Fi network. The Airzone Cloud app can be used to connect Airzone devices to a given network. The Wiser firmware version should not be lower than 3.44. On the Home
Page 334 of 986