Showing 3,421 - 3,430 of 9,859 results

Page 343 of 986
  • Climate

    Wiser Home – System User Guide (France)

    Climate Climate Climate Not all Devices can be added to all Wiser Hubs. To find out if a Device can be added to your Hub, please check chapter Device compatibility list Wiser Radiator Thermostat CCTFR6100CCTFR6101 Provides individual temperature control for radiators. Instruction Sheet (PDF) Device
  • Resolução de problemas

    Plenum Airzone e Aidoo Pro - Ar condicionado – Guia do utilizador do dispositivo Wiser Home

    casa.Se o problema persistir, contacte o Suporte Wiser. Dispositivos não detetados durante o processo de emparelhamento Possível causa:Os dispositivos Airzone não estão ligados ou não estão ligados à mesma rede que o Wiser Hub, ou o dispositivo Airzone não está a ser executado na versão mais
  • Uso del dispositivo

    Schneider Inverter y Boost – Guía del usuario del dispositivo Wiser Home

    tiene un dispositivo de medición de red vinculado al inversor, durante la puesta en marcha el sistema solo mostrará el componente del panel solar del inversor en el sistema Wiser y no mostrará el equipo de red. Si la batería se instala más tarde, tendrá que volver a poner en marcha el sistema "Solar
  • Pairing the device with the Wiser Hub

    Ovalis - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    . Then, scan the QR code located on the device. If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one
  • Anti-Tripping Management

    Odace - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    a defined limit. The limit value is set by your Contract limit, refer to Setting Tariff. Devices that are eligible will be added automatically to the Anti-Tripping Management. When a device is managed by the Anti-Tripping management, the Schedules, Moments and Automations for that device are not
  • About the Document

    Wiser Home – System User Guide (Denmark)

    customization, troubleshooting, and system decommissioning, offering a complete reference for managing a connected home environment. Validity Note This documentation supports the Wiser Home app functionality on following device platforms: Mobile phone/tablet: Android Version 8 and later iPhone/iPod
  • Operar um módulo de botão de pressão

    Sistema M e Sistema D - Botão de pressão conectável simples/duplo – Guia do utilizador do dispositivo Wiser Home

  • Operar um módulo de botão de pressão

    Sistema M e Sistema D - Interruptor sem fios conectável simples/duplo – Guia do utilizador do dispositivo Wiser Home

  • Identifying the device

    Unica - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    Identifying the device Identifying the device Identifying the device Using the Wiser Home app, you can identify a Socket outlet from the other available devices in the room. On the Home screen, tap . Tap Devices Connected Socket Identify (A). This feature flashes the Socket outlet LED, so you can identify the actual device. It may take up to a minute to start and flash the Socket outlet LED. The socket LED will continue to flash until you tap OK.
  • Informações técnicas

      Same topic found multiple times in this document:
    Informações técnicas Tensão de rede: CA 220-240 V, 50 Hz Potência de comutação: 2 (1) A, CA 230 V carga total máx. 2,5 A Esquema de ligação: Apenas cablagem fixa Interface de utilizador: 2x botão de pressão/LED Interfaces com fios: 1x saída de relé, 1x interface de caldeira digital, 1x fonte de
Page 343 of 986