Showing 3,431 - 3,440 of 9,859 results

Page 344 of 986
  • Shutter Group

    LK FUGA Wiser wireless battery 4 button switch – Wiser Home Device User Guide

    Shutter Group Shutter Group Shutter Group A shutter group is a group of shutter devices that are grouped together for a single control. The shutter group can be assigned to the top or bottom push buttons. The shutter group requires two push buttons. You can assign the same shutter group to multiple
  • About the Document

    System M and System D - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    About the Document About the Document About the Document Document Scope This document provides instructions for installing, configuring, and using the System M and System D Connected Single Socket Outlet 16 A with the Wiser Home system. It explains how to pair the device with the Wiser Hub or a
  • Technical data

    Schneider Charge – Wiser Home Device user guide

    (+/- 10%) 50/60 Hz 1–ph Nominal output power 11 kW 16 A (3 P + N) 7.4 kW 32 A (1 P + N) 22 kW 32 A (3 P + N) Cabling Top, back or bottom cabling Embedded protection RCD-DD 6 mA DC filter Maximum supply current 32 A 16 A Socket-outlet type 1 (only T2S) Attached cable Attached cable 5 m or 7 m with T2
  • About the Document

    Unica - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    Note The characteristics of the products described in this document are intended to match the characteristics that are available on www.se.com. As part of our corporate strategy for constant improvement, we may revise the content over time to enhance clarity and accuracy. If you see a difference
  • About the Document

    Wiser Home – System User Guide (France)

    customization, troubleshooting, and system decommissioning, offering a complete reference for managing a connected home environment. Validity Note This documentation supports the Wiser Home app functionality on following device platforms: Mobile phone/tablet: Android Version 8 and later iPhone/iPod
  • About the Document

    Ovalis - Connected Relay Switch 10 A – Wiser Home Device user guide

    About the Document About the Document About the Document Document Scope This document provides detailed information on the Ovalis - Connected Relay Switch 10 A, covering its features, installation, configuration, and operation. It explains how to pair the device with the Wireless switch and Wiser
  • About the Document

    Unica - Connected Relay Switch 10 A – Wiser Home Device user guide

    About the Document About the Document About the Document Document Scope This document provides detailed information on the Unica - Connected Relay Switch 10 A, covering its features, installation, configuration, and operation. It explains how to pair the device with the Wireless switch and Wiser
  • Lights

    Wiser Home – System User Guide (Denmark)

    . LK product catalog Instruction Sheet (PDF) Device User Guide LK Fuga® Wiser Multiwire LED Rotary Dimmer 545D6103 545D0103 Controls the lighting level in a room, or automatically set lighting to a desired level in response to a specified condition or event. Can switch and dim ohmic, inductive or
  • Reading the System User Guide Online

    Wiser Home – System User Guide (France)

    . A Table of Contents Tap/Click to navigate through the topics. Tap/Click the + and - icons to expand/collapse a chapter. B Document name Tap/Click to navigate to the first page of the document. C PDF Icon Tap/Click to open the document as a PDF file. D Search field Enter a search term and tap/click
  • Acerca del dispositivo

    Sensor de temperatura/humedad Wiser – Guía del usuario del dispositivo Wiser Home

    está conectado a Wiser Hub, notifica los datos de temperatura y humedad a Wiser Hub. El sensor activa otros dispositivos Wiser (como un aparato de aire acondicionado si la temperatura es alta o un ventilador extractor si la humedad es alta) a través de la automatización. Características del sensor
Page 344 of 986