Showing 361 - 370 of 1,457 results

Page 37 of 146
  • Unica - Connected Motion Sensor with Switch 10 A

    + 33 (0) 1 41 29 70 00 www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Voice control Voice control Using Amazon Alexa™ or Google Home, you can control the device with your voice. Schneider Electric 35 rue Joseph
  • LK FUGA® Wiser wireless PIR dimmer with neutral

    Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Adjusting the brightness level using app Adjusting the brightness level using app Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500
  • LK® One Wiser Motion Sensor with Switch 10A

    + 33 (0) 1 41 29 70 00 www.se.com Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Voice control Voice control Using Amazon Alexa™ or Google Home, you can control the device with your voice. Schneider Electric 35 rue Joseph
  • Troubleshooting in Quick Home Connect

    Wiser Micro Module Light Switch – Wiser Home Device user guide

    module light switch Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Micro module light switch
  • Troubleshooting in Quick Home Connect

    Wiser Micro Module Shades Control – Wiser Home Device user guide

    module shades control Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Micro module shades
  • Wiser Motion Sensor Wiser Home Device user guide

    triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn On the lights, close the shutter etc. Refer to the AwayMode topic in the respective System User Guide. e.g. Good
  • Setting boost mode manually

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    Setting boost mode manually Setting boost mode manually Setting boost mode manually You can enable and disable boost mode manually.When enabled the temperature increases by 2° C for temperature control modes and by +2 over the setpoint. To enable boost mode: Press the rotary push-button until the
  • Mode silencieux de l’appareil

    Wiser détecteur de fumée sur batterie – Guide de l'utilisateur de l’appareil Wiser Home

    Mode silencieux de l’appareil Mode silencieux de l’appareil Mode silencieux de l’appareil Désactiver les détecteurs de fumée Lors d’un événement d’alarme, identifiez d’abord les détecteurs de fumée qui ont détecté de la fumée, ceux-ci auront des LED rouges clignotants. Appuyez ensuite brièvement
  • Setting RL-LED mode

    Wiser Micro Module Dimmer – Wiser Home Device user guide

    Setting RL-LED mode Setting RL-LED mode Setting RL-LED mode You can change the dimming mode in the app if you have problems with light flickering. By changing the dimming mode, the dimming quality is also improved. On the Home screen, tap . Tap Devices Micromodule Dimmer . Tap the toggle switch (A) to enable the RL-LED Mode.
  • Selecting the operating mode

    Wiser Window/Door Sensor – Wiser Home Device user guide

    Selecting the operating mode Selecting the operating mode Selecting the operating mode Using the Wiser Home app, you can select the operating mode for the sensor such as window or door. On the Home screen, tap icon. Tap Devices Window/Door Sensor Operation Mode (A) to select one of the following
Page 37 of 146