Showing 3,761 - 3,770 of 9,859 results

Page 377 of 986
  • Skapa ett schema/evenemang

    Renova – Uppkopplad rums-/golvtermostat 16 A – Användarhandbok för Wiser Home-enheter

    på . Tryck fliken > . På sidan Ny tidplan sidan anger du Schemanamn, välj TYPoch välj rum. Tryck på Skapa. Välj en valfri dag (A) och tryck på för att lägga till en händelse: TEMPERATURER: Välj önskad temperatur (till exempel 16 °C). Om du drar skjutreglaget till botten av tidslinjen för schemat
  • About the Document

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    About the Document About the Document About the Document Document Scope This document provides the information about the installation, configuration, and usage of the Exxact - Connected Thermostat Room/Floor 16 A. It explains device features such as temperature control, preset modes, manual and app
  • About the Document

    Wiser Home – System User Guide (Spain and Portugal)

    customization, troubleshooting, and system decommissioning, offering a complete reference for managing a connected home environment. Validity Note This documentation supports the Wiser Home app functionality on following device platforms: Mobile phone/tablet: Android Version 8 and later iPhone/iPod
  • Trends

    Wiser BMS – Building Management System – User Guide

    . Trend charts are a way to graphically present trend logs. A trend chart can contain one or more trend logs that are represented by lines or bars. You can also add and remove trend logs from a trend chart. This makes it easy to compare different trend logs. On the Home screen, click Trends. On the
  • Acerca del dispositivo

    Schneider Charge – Guía del usuario del dispositivo Wiser Home

    Acerca del dispositivo Acerca del dispositivo Acerca del dispositivo Schneider Charge ofrece a los propietarios de viviendas una forma fácil e inteligente de cargar sus vehículos eléctricos. La aplicación Wiser Home permite un fácil acceso para supervisar y controlar la experiencia de carga a
  • Skapa ett schema/evenemang

    Exxact – Uppkopplad rums-/golvtermostat 16 A – Användarhandbok för Wiser Home-enheter

    på . Tryck fliken > . På sidan Ny tidplan sidan anger du Schemanamn, välj TYPoch välj rum. Tryck på Skapa. Välj en valfri dag (A) och tryck på för att lägga till en händelse: TEMPERATURER: Välj önskad temperatur (till exempel 16 °C). Om du drar skjutreglaget till botten av tidslinjen för schemat
  • Anti-Tripping Management

    Unica - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    a defined limit. The limit value is set by your Contract limit, refer to Setting Tariff. Devices that are eligible will be added automatically to the Anti-Tripping Management. When a device is managed by the Anti-Tripping management, the Schedules, Moments and Automations for that device are not
  • Configurar o comportamento do indicador LED

    . Selecione o dispositivo que pretende atualizar e toque em Comportamento do indicador LED. Se não conseguir encontrar esta opção na sua aplicação, reponha o dispositivo para a predefinição de fábrica e execute o processo de emparelhamento. Selecione uma das seguintes opções de acordo com a sua
  • Uso del dispositivo

    Micro módulo regulador Wiser – Guía del usuario del dispositivo Wiser Home

    del dispositivo muestra las siguientes opciones: A Arrastre la barra deslizante hacia arriba/hacia abajo para aumentar/reducir el brillo. B Pulse para encender/apagar manualmente el dispositivo. C Pulse para volver a la pantalla Programación horaria, donde puede crear un calendario. Para obtener más
  • Datos técnicos

    Termostato de radiador Wiser – Guía del usuario del dispositivo Wiser Home

    control < 0,8 °C a 4 °C/h Temperatura superficial en el lugar de instalación máx. 93 °C Temperatura del agua máx. 110 °C, máx. continuo 73 °C Temperatura ambiente de funcionamiento De 0 °C a 45 °C Temperatura de almacenamiento De -20 °C a 65 °C Frecuencia de funcionamiento 2,4 GHz Potencia máx. de
Page 377 of 986