UG_Wiser Building Management System_WH-00

Trends

The Trends feature allows you to monitor and analyze the data over time. It helps you track various parameters, such as temperature, and energy consumption. By visualizing this data, you can identify patterns, problems, and make better decisions to improve building operations.

Trend charts are a way to graphically present trend logs. A trend chart can contain one or more trend logs that are represented by lines or bars.

You can also add and remove trend logs from a trend chart. This makes it easy to compare different trend logs.

  1. On the Home screen, click Trends.

  2. On the left pane, you can see the following options:

    • Trend Log Chart

    • Trend Log List

Trend Log Chart

The Trend Log Chart displays recorded data in a graphical format. This feature is particularly useful for visualizing trends and changes over a period of time. You can add multiple trend logs to a single chart, allowing you to compare different data sets, such as energy consumption versus average temperature. This helps you spot correlations and significant events more easily.

Here is an example of a Time vs. Set point temperature Trend Log Chart.

  • When you hover over the graph, you can see the temperature of the assigned room, as well as the time and date.

  • When you click Show legend, you can see the room numbers with the colored boxes.

  • When you click Hide legend, it will be hidden, and the graph will be visible.

Trend Chart Toolbar

The Trend Chart Toolbar allows you to manage and interact with trend charts easily.

Save

Save the changes to the chart.

Zoom to fit

Displays the complete data within the visible area.

Zoom tool

Increase the scale of the trend chart or drag to magnify an area in the trend chart.

Pan tool

Move the chart horizontally to see data that is not currently visible.

Hour

Set the scale of the x-axis to one hour.

Day

Set the scale of the x-axis to one day.

Week

Set the scale of the x-axis to one week.

Month

Set the scale of the x-axis to one month.

Year

Set the scale of the x-axis to one year.

Go to date

Set the scale of the x-axis to the selected date.

Show events

Displays the events.

Show alarm guides

Displays the alarm lines on the graph.

Settings

Allows you to configure the trend chart series, axes, and calculations.

Automatic scroll

The chart updates with the latest data by automatically scrolling to the most recent values.

Show tool tip for the closet item

Displays the values of the series only where the cursor is placed.

Show tool tip for all series

Displays the values of all series for the timestamp where the cursor is placed.

Show as list

Displays all trend chart series as a list for each timestamp.

Trend Log List

The Trend Log List shows all recorded values with their timestamps. You can view, edit, and export this data to excel or .csv for analysis. It's useful for detailed inspections and reporting, giving you a complete record of all monitored parameters.


Exporting a Trend Log List to excel

You can export a trend log list to excel format for viewing and processing.

  1. On the Home screen, click Trends.

  2. On the left pane, click Trend Log List.

  3. On the Trend Log List toolbar, click Export to Excel.

    The Export to Excel pop up appears.

  4. Select the Start (R) and End (S) date.

    TIP: If you want to include the placeholder values, tick the checkbox.
  5. On the top right pane, click Export (T).

    You have successfully exported the trend log list to excel format.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.