DUG_Exxact – rums-/golvtemostat 16 A_WH-00

Creating a Schedule/Event

The device can be fully controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.

To create the schedule/event:

  1. On the Home screen, tap .

  2. Tap on the Schedules tab > .

  3. On the New Schedule page, enter the Schedule name, select Type, and select room.

  4. Tap Create.

  5. Select any day (A) and tap for add event:

    • Select temperature (for example 16 °C).

    • Set time (for example 12:00).

      OBS: A maximum of 8 events can be created per day.

      You can tap to copy the schedule from one day to other days or copy the entire schedule to a new schedule or to an existing one.

  6. Tap Set.

  7. On the top right corner of the screen, tap and select Follow schedule toggle switch to turn on/off the schedule.

When your system is following a schedule:
The new set point will continue to be active until the next scheduled event.

You can see the until time on the Control tab under the device name. The until time shows the time till which the schedule is set to ON.


When your system is not following a schedule:
Any set-point changes made with the slider will continue to be active until the next time the slider is used.
The until time disappears from the screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Var det här till hjälp?