Showing 4,701 - 4,710 of 9,846 results

Page 471 of 985
  • Pairing the device with the Wiser Hub

    System M and System D- Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options: (A): Enter the MAC Address and Install Code, then tap
  • About the Wiser BMS

    Wiser BMS – Building Management System – User Guide

    About the Wiser BMS About the Wiser BMS About the Wiser BMS The Wiser Building Management System (hereinafter referred to as BMS) is a solution to improve the efficiency and effectiveness of buildings equipped with the Wiser system. Wiser BMS allows setting up schedules for lighting, HVAC, and
  • About the Document

    Exxact - Connected Motion Sensor with Multiwire Dimmer – Wiser Home Device user guide

    characteristics that are available on www.se.com. As part of our corporate strategy for constant improvement, we may revise the content over time to enhance clarity and accuracy. If you see a difference between the characteristics in this document and the characteristics on www.se.com, consider www.se.com to
  • Exxact - kaksoispistorasia 16A Wiser Home -laitteen käyttöopas

    käytetään suurellakuormituksella (~18 A tai enemmän), mekanismi voi kytkeä pistorasian poispäältä varmistaen ylikuormitussuojauksen. Pistorasian ominaisuudet:• Etäkäyttö: voit kytkeä pistorasian päälle/pois sovelluksen avulla, yhdistetyn langattoman kytkimen avulla tai ääniohjauksella (Google Home
  • Acerca del documento

    Alarma de humo Wiser - 230V – Guía del usuario del dispositivo Wiser Home

    profesionales cualificados deben demostrar un amplio conocimiento en las siguientes áreas: Conexión a redes de instalación Conexión a varios dispositivos eléctricos Tendido de cables eléctricos Normas de seguridad, normativas y reglamentos locales sobre cableado RIESGO DE INSTALACIÓN DEL EQUIPO Ponga
  • About the Document

    Wiser Smoke Alarm - Battery – Wiser Home Device user guide

    for constant improvement, we may revise the content over time to enhance clarity and accuracy. If you see a difference between the characteristics in this document and the characteristics on www.se.com, consider www.se.com to contain the latest information. For your safety EQUIPMENT INSTALLATION
  • eSetup Commissioning- International

    EVlink Home Smart – Wiser Home device user guide

    eSetup Commissioning- International eSetup Commissioning- International eSetup Commissioning- International Once the EVlink Home Smart is installed, follow the steps to commission via eSetup app: Open eSetup app and select EVlink Home Smart (A). Power on the EVlink Home Smart charger to activate
  • Creación de una automatización

    Termostato Empotrado Wiser 2 A – Guía del usuario del dispositivo Wiser Home

    Creación de una automatización Creación de una automatización Creación de una automatización Una automatización le permite agrupar varias acciones que normalmente se realizan juntas, que se activan automáticamente o que se activan a horas programadas. Con la aplicación Wiser Home puede crear
  • Identificación del dispositivo

    Unica - Interruptor inalámbrico de una/dos teclas conectado – Guía del usuario del dispositivo Wiser Home

    cortas consecutivas y con gran rapidez del pulsador (A). El interruptor inalámbrico se reactiva durante un minuto y el LED de estado parpadea en verde 5 veces y, a continuación, se para. En la pantalla de Inicio, pulse Dispositivos Interruptor inalámbrico de dos teclas conectado Identificar (A). El LED
  • Controlar o dispositivo com botões de pressão

    Unica - Interruptor sem fios conectável simples/duplo – Guia do utilizador do dispositivo Wiser Home

    interruptor sem fios (< 0,5 s) para ligar/desligar a luz, ou para o definir para um nível de brilho específico (apenas para variadores). Estore Prima ligeiramente o botão de pressão atribuído no interruptor sem fios (< 0,5 s) para abrir/fechar o estore para a percentagem configurada. Momento
Page 471 of 985