DUG_EVlink_WH-07

eSetup Commissioning- International

Once the EVlink Home Smart is installed, follow the steps to commission via eSetup app:
  1. Open eSetup app and select EVlink Home Smart (A).
  2. Power on the EVlink Home Smart charger to activate the Wi-Fi® access point. The Wi-Fi® access point will remain active for 4 minutes, after power On.
  3. Enable Wi-Fi on your smartphone and connect to the EVlink Home Smart via Wi-Fi direct.
  4. In eSetup app, tap Open Settings (B).
  5. Select EVlink Home Smart - International
  6. On the screen enter the New PIN, confirm the PIN and tap Save.
    NOTE: The PIN must contain 6 to 16 digits, cannot contain the same digit more than 3 times, or a suit of 6 digits or more.
    New PIN update is successful.
  7. On the next page, enter the New PIN and tap Connect.
  8. On the firmware page, if EVlink Home Smart firmware is up to date, tap Continue to view Network Settings.
    NOTE: If a new firmware version is available, tap Update and tap OK after the update is done.
  9. In Network Settings page, select the way to connect the EVlink Home Smart to the internet and tap Save and continue.
    IMPORTANT: If you have a Wiser Hub for remote monitoring and control, make sure that both the EVlink Home Smart and the Hub are connected to the same Wi-Fi® network.
    • Wi-Fi (C):Tap on Scan Wi-Fi QR Code and scan the QR code on your router to connect to Wi-Fi automatically. Alternatively, you can choose from the list of available networks by taping Select a network or manually enter the Wi-Fi network name and password.
    • Ethernet (D): Enter the network details to connect (use RJ45 cable type).
  10. In Electrical settings page, select the power rating of the EVlink to match the electric installation. You can use the sliding bar (E) or –/+ to limit the charging current and tap Save and continue (F).
    NOTE: Minimum and maximum charging currents are 10 A and 32 A respectively.

  11. In Device settings page, you can enable or disable the power meter using the toggle switch and than tap Save and continue.
    NOTE: If you enable this option make sure you have connected the power meter to the EVlink Home Smart.
  12. Tap Continue in the Supervision page.
  13. Once all the device settings are configured, tap Handover to customer and share the PIN with the customer.
  14. After sharing the PIN, read the instructions and swipe to navigate to next screen. Tap I understand : restart (G) to restart the EVlink Home Smart.
    Please wait for 5 minutes before EVlink Home Smart connects to the internet router.
    • The LED will slowly pulse light green during 5 minutes.

    • EVlink Home Smart shall be restarted according to the applied configuration.

    NOTE: In case you need to modify the commissioning parameters, you can reconnect to the charging station during the 5 minutes, after restart or power-on.

    The LED will turn to solid green 5 minutes after restart confirming that EVlink Home Smart is successfully connected for remote operation.

    NOTE: The LED pulse light green slowly when the EVlink Home Smart is not connected to the internet.

Use Wiser Home app to monitor and control the EVlink Home Smart.

Refer Pairing the device to pair the device with Wiser Home app.

Refer Using the device to monitor and control with Wiser Home app.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?